Technical FAQs

Ask a Question

What would cause Unity to generate a "Not a Valid Configuration" error after downloading a successfully converted NXT or PW32 application to the PLC?

This error points to a corrupted configuration in the converted file. Even though the file built successfully there is a problem in the configuration which can corrected
by doing the following.

 1:  Remove the IO modules from the IO Map
 1a: Rebuild the application
 1b: Re-enter the modules in the IO Map.

Another possibility 

 2: Remove the communication option modules from the application.
 2a:Rebuild the application
 2c:Re-enter the communication option modules.

 
Was this helpful?
What can we do to improve the information ?