Technical FAQs

Ask a Question

Osisense XU - XUK9T laser sensor for anti-collision mode - Size of the laser light spot

Attached the XUK9TAH2MM12 graph of the laser light spot size, depending on the measurement distance from 0.3m to 70m.

Was this helpful?
What can we do to improve the information ?