Technical FAQs

Ask a Question

On ATV320, why I can not configure STO function to STO+LI3 inputs?

Issue:
On ATV320, why I can not configure STO function to STO+LI3 inputs?
Only the choice LI5-LI6 is available.

Product Line:
ATV320
 
Environment:
 STO function

Cause:
 n/a

Resolution:

To be able to configure STO on STO + LI3, you need first to be sure that no other functions are already configured to another function.
If the LI3 choice does not appear check that LI3 is not already assigned to another function.
 
Was this helpful?
What can we do to improve the information ?