Technical FAQs

Ask a Question

Preventa XY2C - XY2CZ9370 mounting kit composition

Find below the XY2CZ9370 mounting kit composition with dia 3.2mm cable in 70m length, still available to order in 2017, not shown into the Preventa XY2C catalogue; and suitable for the XY2CE rope pull switch (end spring XY2CZ702). Suggested alternative in the current Preventa XY2C catalogue dated on 2016 for the XY2CE = XY2CZ9570

XY2CZ9370 mounting kit composition
- 20 cable supports XY2CZ601
- 1 end spring XY2CZ702
- 1 galvanised cable Ø 3.2 mm - L 70 m (cable length)
- 1 turnbuckle XY2CZ404
- 3 cable end protectors XY2CZ701
- 4 cable grips XY2CZ523
Was this helpful?
What can we do to improve the information ?