Technical FAQs

Ask a Question

Preventa XY2C - XY2CZ9350 mounting kit composition

Attached the old XY2CZ9350 mounting kit composition with dia 3.2mm cable in 50m length, still available to order in 2017, not shown into the Preventa XY2C catalogue; and suitable for the XY2CE rope pull switch (end spring XY2CZ702). Suggested alternative in the current Preventa XY2C catalogue, dated on 2016, for the XY2CE = XY2CZ9550

Was this helpful?
What can we do to improve the information ?