Technical FAQs

Ask a Question

How do I set the ATV630 drive for separate controls Speed reference HMI and Start / Stop terminals? 

Issue:
How do I set the ATV630  drive for separate controls Speed reference HMI and Start / Stop terminals? 

Product Line:
ATV630 

Environment: 
All

Cause:
Terminal Start and HMI Speed Ref

Resolution
Go to Main Menu
Go to Complete Settings 5.0
Go to Command and Reference   5.5 
Go to desired reference channel and set to "Ref Freq / Rmt Term" 
Go to Control mode and set to Separate
Enter
Was this helpful?
What can we do to improve the information ?