Technical FAQs

Ask a Question

What are the part numbers for the HMIDT protective sheets?

Issue:
What are the part numbers for the HMIDT protective sheets?

Product Line:
HMIGTU, HMIDT

Environment:


Cause:


Resolution:
Below are the part numbers for the HMIGT Protective sheets.  It comes in a quantity of 5 peel-off sheets.
HMIDT351 HMIZG63 
HMIDT551 HMIZD65W 
HMIDT651 HMIZD66W 
HMIDT542 HMIZG65 
HMIDT642 HMIZG66 
HMIDT732 MPCYK50SPSKIT
Was this helpful?
What can we do to improve the information ?