Browse FAQs

Osisense XC - What is the head reference of the XCKS131H29 limit switch

Published date: 10 April 2019

To answer to such request, you have to know that Telemecanique Sensors offers 2 models of XCKS limit switch :
- the old one in plastic black colour (body & head) which is sold only in sub-assemblies and in spare parts shown in the Osisense XCKS catalogue (see @ hereafter)
https://download.schneider-electric.com/files?p_Doc_Ref=MKTED210041EN
In this case, XCKS131H29 = ZCKS1H29 body + ZCKD31 head. Lever alone has reference ZCKY31.


- The new one in plastic blue colour for the body and black colour for the head, having integrated contacts. No spare parts available, except the lever (same as the old model). In this case, XCKS131H29 head is not available to order. The head reference ZCKD31 is not compatible with this new head.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.