Technical FAQs

Ask a Question

Does the Sepam series 20 keeps the internal time in case of loss of the auxiliary supply?

Sepam series 20 the internal clock is being kept by a capacitor up to 24 hours after a power outage.

As additional information; the Sepam parameters and protection settings are being saved in a non-volatile memory. Other data are also being saved in the non-volatile memory, and you can see them in the files that I have attached.

AEDL3
Was this helpful?
What can we do to improve the information ?