Technical FAQs

Ask a Question

Video: How do you compare two ProWORX 32 projects?



1- Open the Compare Setup utility. From the main toolbar, go to UTILITIES then COMPARE.
2- Under the Compare Options, select what you want to compare. Or, click the TOGGLE button to select all the compare options.
3- In the “Compare” and “To” option boxes, click the two BROWSE buttons to select the project databases.
4- Click the OK button to start the compare utility.
5- The Compare Results will be shown. A check mark indicates a match. An “X” indicates a mismatch.
6- You can further click on the mismatch options to get full details on what mismatches occurred between the two projects. In this example the only mismatch was the PLC type – Quantum 11302 vs 11303.
Was this helpful?
What can we do to improve the information ?