Technical FAQs

Ask a Question

Does Schneider Electric offer motor type BRS397WS0868 ?

No, motor type BRS397WS0868 is an OEM specific model with unique design features for the OEM machine builder that uses this model.
The model is proprietary to the OEM machine builder and is not available directly from Schneider Electric due to a contractual agreement with the OEM

Customer in need of BSR397WS0868 should contact the OEM machine builder for spares.

 
Was this helpful?
What can we do to improve the information ?