Technical FAQs

Ask a Question

Does Schneider Electric have a white paper on Ethernet broadcast storm mitigation?

Title
White paper on Ethernet broadcast storm mitigation
 
Issue
White paper on Ethernet broadcast storm mitigation
 
Product Line
M580, M340, Quantum
 
Environment
Ethernet networking
 
Cause
N/A
 
Resolution
Yes, attached is a Schneider Electric white paper on Ethernet broadcast storm mitigation. The intent of this paper is to explain what a broadcast storm is and how
it can affect an Ethernet network. Mitigation techniques will be presented which can be used to reduce the chances of a broadcast storm occurring.
A broadcast storm is an Ethernet network-level issue and when dealing with one the whole Ethernet network must be considered.
Was this helpful?
What can we do to improve the information ?