Technical FAQs

Ask a Question

How many simultaneous explicit messaging connections you can have with the BMENOC03x1 as a server?

Issue:
How many simultaneous explicit messaging connections you can have with the BMENOC03x1?

Product Line:
M580, BMENOC0301, BMENOC0321, NOC

Environment:


Cause:


Resolution:
The BMENOC03x1 can support up to 32 explicit messages as a server for Ethernet/IP or Modbus/TCP.

 
Was this helpful?
What can we do to improve the information ?