Technical FAQs

Ask a Question

Osisense XC - Cross-reference of the XCMA1105 limit switch

The XCMA1105 obsolete limit switch is the XCMA110 limit switch supplied with a 5m cable length, instead of 2m. Attached photo of the XCMA110 obsolete limit switch. The cross-reference of the XCMA1105 limit switch is composed of the following sub-assemblies ZCMD21L5 + ZCE10. We can supply a special ZCE10 head in adapted product, similar to the XCMA110 metal end plunger. It is shown in attachment. Special head reference is ZCE10S51, available to order, not in stock. It has a spherical plunger radius of 5mm.

Was this helpful?
What can we do to improve the information ?