Technical FAQs

Ask a Question

How fast can the CM4000T update the analog outputs?

Issue:
A customer would like to know how fast the analog output status for a CM4000T can be updated for use in a high speed application.

Product Line:
CM4000T

Environment:
CM4000 I/O

Resolution:
The analog output statuses are updated once every 100 ms.  If the desired application requires faster update rates the 4000T may not be appropriate.
Was this helpful?
What can we do to improve the information ?