Browse FAQs

Osisense XC - Data sheet of the adapted XCKP2702P20F0 limit switch

Published date: 24 September 2019

Attached the data sheet of the adapted XCKP2702P20F0 limit switch, sold by quantity of 50 under commercial reference XCKP2702P20F0TQ. It is not shown into the Osisense XC catalogue, but it uses the following standard sub-assemblies ZCP27 body + ZCE02 head + ZCPEP20 cable gland entry. "XCKP2702P20F0TQ" reference is available to order in september 2019, without any marketing restriction. It is produced at order reception.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.