Technical FAQs

Ask a Question

Does Power Monitoring Expert (PME) Reporting support multiple time zones

Issue
Large systems with devices in different time zone locals need reporting to reflect time zone location of the device.

Product Line
Power Monitoring Expert
Struxureware Power Monitoring
ION Enterprise

Environment
Multiple time zone installed systems

Resolution
This functionality was added in PME 9.0. 
Any version prior will not support separate time zones.
Was this helpful?
What can we do to improve the information ?