Technical FAQs

Ask a Question

Is there a recommended Ethernet cable for the M580 Ethernet Remote IO?

Title
Recommended Ethernet cable for the M580 Ethernet Remote IO
 
Issue
Recommended Ethernet cable for the M580 Ethernet Remote IO?
 
Product Line
M580 PAC
 
Environment
Unity Pro 11 or higher
 
Cause
N/A
 
Resolution
 From the Modicon M580 Standalone System Planning Guide for Frequently Used Architectures (page 66), CPUs and eX80 EIO adapter modules do not have fiber ports. Therefore, the maximum distance between the CPU and the first drop and between any two contiguous drops is less than 100 m. Recommend using shielded twisted 4-pair CAT5e or greater (10/100 Mbps) cable. (Do not use twisted 2-pair CAT5e or CAT6 cables.)
 
Was this helpful?
What can we do to improve the information ?