Technical FAQs

Ask a Question

Osisense XC - Datasheet of the adapted switch XCMD2115T2SEZ

Attached the datasheet of the adapted switch XCMD2115T2SEZ, using a special cable halogen free for railway equipments, complying to EN 50306 and EN 45545 standards. It is in fact the XCMD2115T2 limit switch suitable for -40°C in operation (SEZ meaning).
Was this helpful?
What can we do to improve the information ?