Technical FAQs

Ask a Question

Osisense XC - Datasheet of the adapted XCMD connection component ZCMC39T2SF

Attached the datasheet of adapted XCMD connection component ZCMC39T2SF, using a special cable halogen free for railway equipments, complying to EN 50306 and EN 45545 standards. This reference is available to order without any restriction. It is not in stock, it is produced at order reception by the assembly plant. It is the same reference as ZCMC39T1SF with a cable of 2m length.
Was this helpful?
What can we do to improve the information ?