Technical FAQs

Ask a Question

Can the PMXNOW0300 be used in a M580 PAC?

Title
PMXNOW0300 in a M580 PAC
 
Issue
PMXNOW0300 in a M580 PAC
 
Product Line
M580 PAC
 
Environment
Unity Pro 11.1
 
Cause
N/A
 
Resolution
 Yes, a M580 with firmware version 2.2 and Unity 11.1 allows the IO mapping of a PMXNOW0300.
 
Was this helpful?
What can we do to improve the information ?