Technical FAQs

Ask a Question

Osisense XS_Datasheet of the proximity sensor XS630B1MAL2TT

Attached the datasheet of the XS630B1MAL2TT adapted sensor, not shown in the Osisense XS catalogue. The TT suffix meaning is extended high temperature range to +85°C in operation (instead of +70°C). The sales of such product are open for all customers in 2016. It is not in stock (manufacture at order reception).
Was this helpful?
What can we do to improve the information ?