Technical FAQs

Ask a Question

Value cannot be null error when opening SQL Server Management Studio

Issue
The following error shows when opening SQL Server Management Studio:

          
          Value cannot be null.
          Parameter name: viewInfo (Micorsoft.SqlServer.Management.SqlStudio.Explorer)


Product Line
SQL Server Management Studio (SSMS)

Environment
Database Engine

Cause
No free space on disk drive.

Resolution
There was zero space available on hard drive.  After removing unnecessary files, SSMS opened properly.
 
Was this helpful?
What can we do to improve the information ?