Technical FAQs

Ask a Question

What is the part number for an Energy Meter bonding plate?

Issue 
When installing an energy meter it may be necessary to use a bonding plate. 

Product Line
PowerLogic Energy Meter 

Environment
Installation, Wiring
 
Cause
If the connections to the meter will be made through more than one metallic conduit, the conduits will require bonding to prevent the hazard of electric shock.
 
Resolution
A bonding plate is available (P/N: EMBOND), or an equivalent means may be used.
 
Refer to Figure 4 on page 3 of the PowerLogic Energy Meter Instruction Bulletin for more information on the use and installation of the bonding plate.

The Energy Meter instruction bulletin can be downloaded at the following link:

http://powerlogic.com/literature/63230-216-201A5.pdf


 
Was this helpful?
What can we do to improve the information ?