Browse FAQs

What are the maximum number of I/O channels that the x80 CRA's support?

Published date: 04 January 2019

Issue
Need to be aware of the limitation to the number of IO Channels that can be configured in an EIO drop.
Product line
Modicon Quantum, Modicon M580, Modicon X80
Resolution
BMXCRA31200-  128 Digital In/Out  -  16 Analog In/Out
BMXCRA31210-  1024 Digital In/Out  -  256 Analog In/Out
BMECRA31210-  1024 Digital In/Out  -  256 Analog In/Out

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.