Technical FAQs

Ask a Question

Video: How to Change the Controller Type in ProWORX 32

This video will show you how to change the Controller Type in ProWORX 32.
In this example we will change the controller type from a Quantum 140CPU11302 to a 140CPU534 PLC.

1 - With the ProWORX 32 project open go to PROJECT then CHANGE PLC TYPE.
2 - Under “Pick a controller” select Quantum 534
3 - Click the NEXT button, then the FINISH button.
4 - Reopen the Configuration window. ProWORX 32 will ask you to save the new configuration. Select the YES button.
5 - The Controller Type has been changed and will now show Quantum 534.
 
Was this helpful?
What can we do to improve the information ?