Technical FAQs

Ask a Question

How does the drive handle time offset of GMT and daylight savings on the web service?

Issue:
GMT time offset and daylight savings management

Product Line:
ATV630, ATV930

Environment:
All models and serial numbers

Cause:
None

Resolution:
The GMT offset and daylight savings time is not managed on the web service with service packs up to and including 1.5 IE11.  
Please check with Schneider Electric for service packs higher than 1.5 IE11.
 
Was this helpful?
What can we do to improve the information ?