Technical FAQs

Ask a Question

Where can I find a Power Monitoring Expert (PME) 8.2 web applications demo site?

Issue:
Is there a PME demo on the internet?

Product Line:
Power Monitoring Expert 8.2

Environment:
Web Applications

Resolution:
Yes, there is a demo site with access to PME 8.2 web applications.

PME 8.2 - http://www.pmedemo.biz/
user:  guest
password: 0

You have a limited view of the web applications with this user account but you can still demo all components of web applications.
Was this helpful?
What can we do to improve the information ?