Technical FAQs

Ask a Question

Why is the content of trip context not same in NFC and Bluetooth?

Because the Micrologic X Control Unit has very little time to store information on the NFC in case of Trip. In Bluetooth, the Control Unit is powered and can provide all the information.
Was this helpful?
What can we do to improve the information ?