Technical FAQs

Ask a Question

What happens if I click on the “Open” or “Close” button? Will it immediately control the Circuit Breaker?

First, you need to have installed the Masterpact Operation Assistant Digital Module in order to enable Circuit Breaker control. If you haven’t, touching the buttons will have no effect (other than saying you need a license). Second, even if the license is active, you will first be prompted for the control password of Micrologic X. And then, as a second safety procedure to prevent accidental commands, you will need to draw a two-line figure displayed on screen.
Was this helpful?
What can we do to improve the information ?