Technical FAQs

Ask a Question

How do I update an IFM module with Ecoreach over the Modbus TCP network ?

The firmware update of IFM modules can be impacted by the Modbus TCP connections due to communication settings.
With Ecoreach firmware upgrade, it is recommended to limit number of IFMs to a maximum of 4 IFMs stacked behind an IFE Gateway or connected to an EGX gateway.
If the network has more than 4 IFMs, users may encounter a higher rate of failures.  In this case, it is better to do a local connection to the IFM.
Was this helpful?
What can we do to improve the information ?