Technical FAQs

Ask a Question

Preventa XCS - What is the first-up time of the XCSDM3 or XCSDM4 magnetic systems

The first-up time ( or TON) of the XCSDM3 or XCSDM4 magnetic systems is closed to 250ms.
Definition of the first-up time : After a power-up, the system is performing self-tests for checking its integrity. The first-up time is the delay, from power-up, after which the system is ready for operation.
Was this helpful?
What can we do to improve the information ?