Technical FAQs

Ask a Question

What are the dimensions of the hole in the end of the shaft on Lexium ILA type motors

There is a pilot hole found in the center of the output shaft of Lexium Integrated Drives type ILA
This pilot hole is DIN 332 - DS M3

This means the hole accepts a 3mm screw.

 
Was this helpful?
What can we do to improve the information ?