Technical FAQs

Ask a Question

Can you make Online changes to the ProWORX 32 program without shutting down the PLC?

Yes you can. You can make Online changes to the ProWORX 32 program without shutting down the PLC. Just remember, the Offline program will not be updated. If you want the PLC program and Offline project to match, do a Read from Controller.

Was this helpful?
What can we do to improve the information ?