Technical FAQs

Ask a Question

The Magelis loses the event logs message from the Event Summary object on power cycle. How to resolve the issue?

Issue:
The Magelis loses the event logs message from the Event Summary object on power cycle.  How to resolve the issue?

Product Line:
Vijeo Designer, EventLog

Environment:


Cause:


Resolution:
If you are running Vijeo Designer v6.2 and powercycle the Magelis target and loses the event log messages from the Event summary object.  If the Eventlog is set up to back up to SRAM & File.   This was an known issue and was fixed in SP4.1.  
Please use the Schneider Electric Software Update Tool (SESU) to upgrade the SP4.1.  Or contact Schneider Electric Customer Care for a link to download the service pack.
Was this helpful?
What can we do to improve the information ?