Technical FAQs

Ask a Question

Osisense XS - Outer sheath diameter of the XSAV11373 and XSAV12373 proximity sensors

XSAV11373 & XSAV12373 proximity sensors use black PvR cable jacket with 3 wires section 0.34mm2. External diameter of the cable jacket = 4.2 mm +/-0.1mm.
Was this helpful?
What can we do to improve the information ?