Browse FAQs

What driver is needed to connect to an M340 with a third party HMI over Ethernet?

Published date: 30 May 2019

Issue
Connect third part HMI

Product Line
Modicon M340

Resolution
To connect to the M340 with a third party HMI over Ethernet, it will need to use a Modbus TCP/IP driver. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.