Technical FAQs

Ask a Question

Is the Enercept Meter consider a sub meter?

Title
Is the Enercept Meter consider a sub meter?

Issue
Need to know if the enercept meter is consider a sub meter

Product Line
Enercept Meter

Emvironmet
Sub Metering

Cause
Unable to determine if the enercept meter is consider a sub meter

Resolution
Yes, the enercept meter is consider to be a sub meter. Please look at the attached screen shot
for a descptiption of the enercept meter listed on the Schneider Electric Digest 177




 
Was this helpful?
What can we do to improve the information ?