Technical FAQs

Ask a Question

What is the Generated BACnet Tag Format in Scada

Issue
What would be the format of tags after importing

Product Line
PowerScada Expert 8.1

Environment
Import Variable Tags utility in Citect Explorer

Cause
Importing tags for a BACnet device.

Resolution

Generated tag names have the following format:

     <I/O device name><object type><object instance><property type>

For example:
     IODevice1AI12PresentValue

Where:
- I/O device name: IODevice1
- object type: AI (Analog Input)
- object instance: 12
- property type: PresentValue
 
Was this helpful?
What can we do to improve the information ?