Technical FAQs

Ask a Question

Does OFS support Unity Pro native tag such as String, DATE, TIME, DT and TOD?

Currently no.  OFS3.60 supports also theses features by setting OFS internal key in \ProgramData\Schneider Electric\OFS\3.60.0.0\ofsinternal.xml

OFS3.70 will support officially Unity PRO native types (that is String, DATE, TIME, DT and TOD are converted to the IEC 1131-3 formatted value string )

 
Was this helpful?
What can we do to improve the information ?