Technical FAQs

Ask a Question

How to Search the Network for Any Connected FieldServers?

Issue
Finding FieldServer gateways installed on the network.

Product Line
FieldServer Gateway

Environment
Browser based

Cause
Diagnose a problem with FieldServers.

Resolution
FieldServer protocol gateway has a utility called FieldServer Toolbox.  Once installed it makes it easy to check the status and diagnose any FieldServer for network settings, node information and transfer files.  The utility can be downloaded from SMC and also attached to this article.
 
Was this helpful?
What can we do to improve the information ?