Technical FAQs

Ask a Question

Can we configure BMECXM0100 in M580 Hot Standby PLC

The CXM can’t be configured in the M580 HSBY CPUs BMEH582040, BMEH584040 and BMEH586040
Was this helpful?
What can we do to improve the information ?