Browse FAQs

Why can I not change the I/O base in the configuration of a Momentum in EcoStruxure Control Expert (formally Unity Pro)?

Published date: 30 April 2019

Issue
Change the I/O Base on the Momentum 

Product Line 
Modicon Momentum

Enviroment
EcoStruxure Control Expert

Resolution
At the moment, Unity Pro does not have the capability to change the I/O base in a Momentum project once it has been created. If you need to change the I/O base you must create a new project with the correct I/O base, then export logic and variables from the old project and import into the new project. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.