Technical FAQs

Ask a Question

Com'X Device Stuck in Initial Boot Sequence with Amber LED

Issue:
When initially starting up a Com'X device, it remains in the startup phase with an amber power/status LED.

Product Line:
Com'X 200, 210, 510

Environment:
Communication Hardware

Cause:
Com'X device is provided with power and begins the power up sequence; however, the power/status LED remains amber even after the suggested 8-12 minute time frame. This can occur on brand new devices.

Resolution:
*Warning: performing a factory reset will erase all stored data and logs.

Please complete a factory reset on the Com'X device as per the Com'X Installation Guide (FA289876) page 7.
Reset steps can also found in KB article FA228712.

Note: if powering the Com'X via PoE, it cannot be disconnected from the network as this its source of power. Follow the remaining steps for resetting and the device should complete its startup.
Was this helpful?
What can we do to improve the information ?