Browse FAQs

Quantum Loss of Ethernet IO drop after reboot.

Published date: 08 November 2018


Issue
Quantum Loss of Ethernet IO drop after reboot.
 
Product Line
Quantum Ethernet IO
 
Resolution
This issue was addressed with Unity Pro Hotfix (HF0348186R). It is available on the shopping Kiosk and at SE.com.
UnityPro_V100_HF0348186R fixes the following issue: On Quantum Application, if NRP module  is used on EIO DROP (Quantum DROP), when a drop is modified, after upload of the application on the PC,. some part of application are built but other not, which causes inconsistencies.

This patch is also available for Unity Pro V11 and 11.1 and the issue was finally resolved beginning with Unity v12. A build of the project is required to recover.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.