Technical FAQs

Ask a Question

Osisense XS - What plastic is the fixing clamp XSZB104 or XSZB105 made of

The fixing clamps XSZB104 & XSZB105 are made of black PA66/6 GF30. GF30 means 30% glass fiber reinforced. PA66/6 stands for Polyamide 6.6 + Polyamide 6 blend (Example of trade name Ultramid).

Was this helpful?
What can we do to improve the information ?