Technical FAQs

Ask a Question

Osisense XS - What plastic is the reference XSZA020 or XSZA034 made of?

The adaptor collar Ø 20 mm (XSZA020) or Ø 34 mm (XSZA034) for XS or XT proximity sensors, is made of PBT. PBT stands for Polybutylene Terephthalate. Example of PBT trade name = Crastin PBT.

Was this helpful?
What can we do to improve the information ?