Technical FAQs

Ask a Question

What is the meaning of error EC10 in Unity using a Modicon M580 controller?

Title
Meaning of Unity error EC10
 
Issue
Meaning of error EC10 in Unity
 
Product Line
M580 PAC
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 The Unity error EC10 indicates an attempt was made to read or write to an undefined area with in the M580 CPU.
This problem was corrected in the M580 CPU firmware version 2.20.
Was this helpful?
What can we do to improve the information ?