Technical FAQs

Ask a Question

Osisense XU - Datasheet of XUM9APCNL03M12 photoelectric sensor

Any specific data sheet of the adapted XUM9APCNL03M12 photoelectric sensor, does not exist. The commercial reference XUM9APCNL03M12 is a standard product XUM9APCNL2 (cable 2m length), supplied with a 30cm pigtail having a M12 connector 4-pin. Attached the M12 connector pin-out. Standard reference data sheet in the following @ http://www.tesensors.com/datasheet/XUM9APCNL2/


 
Was this helpful?
What can we do to improve the information ?