Technical FAQs

Ask a Question

Osisense XM - Cross-reference of the discontinued reference XMLC035C2S11

XMLC035C2S11 pressure switch reference can be replaced by the XMLC035C2S12. Both references have the same fluid entry, technical difference is the electrical cable entry only : S11 = Pg 13.5, S12 = ISO M20x1.5. Corresponding datasheet @ http://www.tesensors.com/datasheet/XMLC035C2S12/
Was this helpful?
What can we do to improve the information ?